Command/Query
:CALCulate:TRACe{Tr}:GATE:STARt <numeric>
:CALCulate:TRACe{Tr}:GATE:STARt?
This command sets start value for the gating function.
|
Description |
Starting point of the gate |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
- |
|
Preset Value |
-10n |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":CALC:TRAC1:GATE:STAR 2e-9"
20 OUTPUT 717;":CALC:TRAC1:GATE:STOP 6e-9"
30 OUTPUT 717;":CALC:TRAC1:GATE:TYPE BPAS"
40 OUTPUT 717;":CALC:TRAC1:GATE:STAT ON"
50 OUTPUT 717;":CALC:TRAC1:GATE:STAR?"
60 ENTER 717;A
:CALCulate:TRACe{Tr}:GATE:STOP
:CALCulate:TRACe{Tr}:GATE:TYPE
:CALCulate:TRACe{Tr}:GATE:STATe
TDR/TDT > Gating > Start virtual knob OR
TDR/TDT > Gating > type in the text box under the Start virtual knob OR
Right-click on the time domain graph plot and select Set Gating Range